Environmental Conditions
Ambient Temperature
-
Operation temperature
-
–25 to +70 °C (–13 to +158 °F): Normal operating temperature
NOTE: The minimum operating temperature for the earth-leakage fault indicator on the MicroLogic 4 and 7 trip unit is -15 °C (5°F). Between -15 and -5 °C (5 and 23 °F), and when operating the device with an earth leakage fault and a very low load compared to the trip unit rating In, the earth leakage indicator may not work correctly (fault indication or reset). -
–35 to –25 °C (–31 to –13 °F): Commissioning possible
-
-
Storage temperature
-
–50 to +85 °C (–58 to +185 °F): Without MicroLogic trip unit
-
–40 to +85 °C (–40 to +185 °F): With liquid crystal MicroLogic trip unit or PowerTag Energy
-
Extreme Atmospheric Conditions
They are tested for extreme storage conditions according to the following standards:
Standard |
Title |
---|---|
IEC/EN 60068-2-2 |
Dry heat, severity level +85 °C (+185 °F) |
IEC/EN 60068-2-1 |
Dry cold, severity level –55 °C (–67 °F) |
IEC/EN 60068-2-30 |
Damp heat, cyclic
|
IEC/EN 60068-2-52 |
Salt-mist test |
To obtain the best use from the circuit breakers, install them in properly ventilated switchboards where excessive dust is not a problem.
Vibration
Conformity tests are carried out in accordance with standard IEC/EN 60068-2-6 at the levels of severity required by the merchant shipping regulatory bodies (IACS, Veritas, Lloyd namely):
-
2 Hz to 13.2 Hz with an amplitude of +/- 1 mm (+/- 0.04 in)
-
13.2 Hz to 100 Hz at a constant acceleration of 0.7 g
Electromagnetic Disturbances
They comply with the requirements of the electromagnetic compatibility (EMC) standard:
Standard |
Title |
---|---|
IEC/EN 60947-2 appendixes F and J |
Overcurrent protection tests |
IEC/EN 60947-2 appendixes B and J |
Specific tests for earth-leakage protection |
Check for compliance with EMC standards by testing for immunity to:
-
Overvoltages produced by the operation of electromagnetic switchgear.
-
Overvoltages produced by atmospheric disturbance that pass through the electrical network (for example, lightning).
-
The use of apparatus emitting radio waves (such as radio transmitters, walkie-talkies, or radar).
-
Electrostatic discharges produced by the operators themselves.
Conformity with EMC standards as described above helps to ensure that:
-
The circuit breaker operates correctly in a disturbed environment:
-
Without nuisance tripping.
-
In accordance with the trip time.
-
-
There is no disturbance to any type of industrial or commercial environment.
Altitude
Above 2,000 m (6,600 ft) modifying the characteristics of the surrounding air (dielectric strength, cooling capacity) causes derating as follows:
Altitude (m/ft) |
< 2,000 m (6,600 ft) |
3,000 m (9,800 ft) |
4,000 m (13,000 ft) |
5,000 m (16,500 ft) |
---|---|---|---|---|
Maximum operating voltage (V) |
690 |
590 |
520 |
460 |
Maximum operating voltage (V) for NSX400K |
1000 |
886 |
790 |
696 |
Rated thermal current (A) at 40 °C (104 °F) |
In |
0.96 x In |
0.93 x In |
0.9 x In |