Troubleshooting
Introduction
Troubleshooting operations are described in the following tables, with the checks or repairs to be carried out in relation to the probable causes of the malfunction indicated. They are classified into the following events:
-
Repetitive tripping
-
Circuit breaker fails to close (manually operated circuit breaker)
-
Circuit breaker fails to close (motor-operated circuit breaker)
-
MicroLogic 5, 6 and 7 fault screens
Repetitive Tripping
Indication |
Probable cause |
Checks or repairs |
---|---|---|
SD |
Supply voltage to the MN undervoltage trip release is too low or subject to significant variations |
Check the power supply for the release (for example, a supply powering motors with high power ratings may be unstable). If so, connect the release to a clean or stable supply. |
Supply voltage to an MX shunt trip release applied unintentionally |
Check that the release connection is correct compared to the installation diagram. |
|
SD, SDE |
Operating temperature too high |
Check the switchboard ventilation and the temperature in the room. |
SD, SDE, SDV Earth-leakage fault indicator (MicroLogic 4) Information on display screen (MicroLogic 7) Button R on VigiPacT Add-on in the out position (MicroLogic 5 and 6 with VigiPacT Add-on) |
Inappropriate earth-leakage protection setting (MicroLogic 4 and 7 or VigiPacT Add-on) |
Check the value of the natural leakage current. Depending on the results:
|
Transient insulation fault on the equipment |
Check whether the fault coincides with commissioning an item of equipment. Depending on the results:
|
|
SD, SDE Screen (available only in MicroLogic 5, 6, and 7) then |
Operating temperature too high |
Check the switchboard ventilation and the temperature in the room. |
Circuit Breaker Fails to Close (Manually Operated Circuit Breaker)
Indication |
Probable cause |
Checks or repairs |
---|---|---|
SD |
MX shunt trip release energized MN undervoltage trip release not energized |
Check that the release connection is correct compared to the installation diagram. |
OF |
Circuit breaker interlocked |
Check the installation and interlock diagram (mechanical or electrical) for both circuit breakers. |
Circuit Breaker Fails to Close (Motor-Operated Circuit Breaker)
Indication |
Probable cause |
Checks or repairs |
---|---|---|
OF |
Close instruction not operational |
Check the Auto position of the selector on the front of the circuit breaker. Also check:
|
MicroLogic 5, 6, and 7 Fault Screens
The following table shows the checks or repairs to be carried out according to the MicroLogic 5, 6, and 7 fault screens. For more information, refer to DOCA0141EN, ComPact NSXMicroLogic 5/6/7 Electronic Trip Units - User Guide.
Indication |
Probable cause |
Checks or repairs |
||
---|---|---|---|---|
Screen then |
Serious fault on the MicroLogic trip unit: the trip unit can no longer provide protection |
Change the trip unit urgently. The circuit breaker cannot be reset. |
||
Screen |
Fault on the MicroLogic trip unit |
Change the trip unit on the next maintenance visit. The trip unit can still provide protection. |
||
Screen |
Acknowledgment of a latching alarm which has not been reset on the SDx module |
Check the cause of the alarm and use the OK button to carry out the reset. |