DOCA0140EN-03

Service Interface Connected to a PC

Description

Use the Service Interface connected to a PC running EcoStruxure Power Commission software to carry out the complete range of checks, tests and adjustments on the MicroLogic trip unit.

Connect the Service Interface to the test port on the front face of the MicroLogic trip unit.

NOTE: The Service Interface cannot be used with the MicroLogic 2.3 trip unit installed in a ComPact NSX400K circuit breaker.

Connection

  1. AC/DC power

  2. 7-pin cable connected to the test port on the trip unit

  3. USB cable with magnet

For more information, refer to .

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?