DOCA0098EN-11

Start Up Your Com’X

The Com’X takes time to start up. Wait for the power LED to turn green before performing any actions.

Once the Com’X is started, most configuration modifications are taken in account without a reboot.

Reboot Cases

The Com’X requires a reboot in the following cases:

  • Upgrading the firmware.
  • Restoring a configuration.
  • Changing the Ethernet network settings between 2 switched ports and 2 separate ports.
  • Inserting a GPRS or 3G modem.
  • Installing a Zigbee key.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.