DOCA0098EN-11

Account Lockout Policy

Account lockout feature disables a user account when the number of failed login attempts exceeds the set limit within a predetermined time interval. This feature is enabled by default.

You can configure the following:

  • Enable account lockout ­ Account lockout policy is enabled by default. Select No to disable this feature. It is recommended to keep the Account Lockout feature enabled to secure the device from unauthorized access.

  • Reset account lockout counter (number of attempts) ­ determines the number of invalid login attempts allowed before user account gets disabled. The default is set to 10 attempts.

  • Account lockout duration (minutes) ­ determines amount of time user account remains disabled. The default is set to 15 minutes.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.