DOCA0098EN-11

Commissioning Overview

The Commissioning tab allows you to view configuration notifications and commission other features.

Commissioning allows you to:

  • check that configuration is completed.
  • start/stop data logging.
  • send the metering architecture to Energy Operation. This option is available only if Energy Operation is selected as the publication platform.
  • export the logged data manually to the selected hosted platform.
  • start the periodic publication of data to the selected hosted platform.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.