DOCA0098EN-11

Modbus Serial Port

The RS-485 serial line standard is an industrial standard.

If configured correctly, it can potentially reduce transmission errors even in an environment with electrical disturbances. This section describes the serial line properties of the local Modbus/RS-485 network controlled by the Com’X.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.