DOCA0098EN-11

Wi-Fi Access Point Settings

The USB Wi-Fi key can be used as a temporary communication medium during the commissioning phase.

This allows you to use a laptop or a tablet to configure the Com’X.

In this case, communication is direct between the Com’X and the laptop or tablet. The Com’X functions as a Wi-Fi access point.

Wi-Fi access can be added to the Com’X using a Wi-Fi USB key inserted under the cover or on the front face. It is recommended to use the front face USB, as you can easily remove the USB key after configuration is done.

Installing the Wi-Fi USB key directly on a Com’X port is allowed only for temporary access point connection for configuration.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.