DOCA0098EN-11

Custom Modbus Device

After you create a custom Modbus device in the Custom Library, you can add it to your network in the same way you add any Modbus device.

You can add a custom Modbus device either by discovering connected devices or by adding a Modbus device manually.

see** Discovering Connected Devices, or by Adding a Modbus Device Manually.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.