DOCA0098EN-11

Custom KYZ Pulse Meter Model

The custom KYZ pulse meter model has a dry contact closure that changes state each time the counter advances.

The Com’X detects the change of state, and the counter increases by the pulse weight value.

Each instance of a custom KYZ pulse meter needs to be directly connected to the digital inputs of the Com’X.

Measurement Properties

The custom KYZ pulse meter model presents the same Measure Properties and Measurements table items as a Custom Pulse Meter.

The measure properties include the following:

Field Description
Count element Select a measure element from the list, or select Custom and type a personalized name into the Custom count element field.
Count unit Select a measure unit from the list, or select Custom and type a personalized unit into the Custom count unit field.
Pulse weight The pulse counter increases by this value each time a pulse is received. The list is restricted to the values that correspond to the selected meter type.
Upper Range

Defines when the active energy counter rolls back to zero.

Flow element Select a flow element from the list, or select Custom and type a personalized name into the Custom flow element field.
Flow unit Select a flow unit from the list, or select Custom and type a personalized unit into the Custom flow unit field.

Index Counter

This graphic shows the difference between a KYZ pulse meter and a standard pulse meter (pulse weight = 10):

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.