DOCA0098EN-11

Custom Main Meter Model

The custom main meter model is made up of two pulse outputs and four contact outputs.

You can create a customized main meter by entering customized settings for the following measure properties of each of the two pulse outputs:

  • Count element
  • Count unit
  • Flow element
  • Flow unit

The signal properties of the four contact outputs present the same configuration choices as the Schneider Electric standard main meter.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.