DOCA0098EN-11

Custom Pulse Meter Model

You can create a customized pulse meter.

To create a customized pulse meter input customized settings for the following measure properties:

  • Count element
  • Count unit
  • Flow element
  • Flow unit

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.