DOCA0098EN-11

Custom Pulse Meter

You can add a pulse meter that is based on a custom pulse meter model.

Before adding a custom device, you first need to create the custom model in the Custom Library.

** (Custom Models)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.