DOCA0098EN-11

Email Service

Configure the Com’X to send emails to deliver periodic data publications and custom event notifications.

NOTE: Contact your network administrator to determine the correct IT connection for port, LAN connection to Internet, and email server to use.
  • Com’X sends an email to the configured email server/MTA (Mail Transfer Agent) using SMTP protocol.

  • MTA forwards the message to the email client MDA (Mail Delivery Agent).

  • MDA delivers email to the client/MUA (Mail User Agent) using POP3 or IMAP protocol.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.