DOCA0098EN-11

Com’X 510 for Entry-level Energy Management

The Com’X 510 supports real-time data views from many common device types, providing several device-specific features.

Additional energy management capabilities include:

  • View real-time and historical information from multiple locations through a supported web browser.
  • Select the logging intervals and topics you want logged.
  • Automatically export selected logged data to your PC for additional analysis.
  • Provide data and system security through password protection and controlled access to individual web pages, as well as through Com’X 510 firewall management.
  • Perform simple control reset commands for supported devices (for example, min/max and accumulated energy).
  • Set date and time for connected devices that support set time commands.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.