DOCA0098EN-11

Main Features

The main features of the Com’X 510 are:

  • real-time data in easy to understand views
  • dashboard view for historical reporting
  • automatic discovery of connected Modbus devices
  • connectivity to the cloud through three media: GPRS/3G, wired Ethernet, or Wi-Fi Ethernet
  • two Ethernet ports to separate upstream cloud connection from field device network
  • four supported transfer protocols: HTTP, HTTPS, FTP, and SMTP with proxy management
  • data logging
  • data export with native connection to Schneider Electric service platforms (such as Energy Operation) and with .csv file for other database servers
  • gateway functionality Modbus TCP to Modbus RTU or Modbus ASCII
  • setup through on-board web pages
  • compliant with electrical switchboard environment (temperature, electromagnetic compatibility)
  • local backup of configuration parameters
  • ZigBee Pro with EM4300 sensors

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.