DOCA0098EN-11

Product Overview

The Com’X 510 energy server is a compact plug and play gateway and data logger and is an essential part of an entry level energy management system.

It collects and stores consumption of WAGES (Water, Air, Gas, Electricity, and Steam) and environmental parameters such as temperature, humidity, and CO2 levels in a building. The Com’X 510 provides access to reports such as on-board device and circuit summary pages, as well as on-board data logging. Data can be securely accessed in real time or transmitted as a report to an Internet database server.

Data is ready to be processed once received by the server. Data is displayed as web pages through energy management services provided by Schneider Electric, such as EcoStruxure™Energy Operation and EcoStruxure™ Facility Expert, to support optimization of energy performance and cost management.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?