DOCA0098EN-11

Save the Configuration

The configuration of a Com’X can be saved to a file and used to restore the configuration on the same Com’X.

You should save a backup configuration before and after each firmware upgrade.

Backup files contain sensitive information such as network passwords. Safeguard the media after the backup in a protected location to prevent unauthorized access.

NOTICE
Hazard of unauthorized access
Do not communicate a backup file to unauthorized persons.
Failure to follow these instructions can result in equipment damage.

The file name is in the format Com’X name_Firmware version_YYYYMMDD-HHMM.zip. For example, MyComXEnergyServer_V6.0_20190110_1020.zip indicates that the file is generated from:

  • a Com’X named MyComXEnergyServer
  • running on the firmware version 6.0
  • on January 10th, 2019 at 10:20 a.m.

The configuration should be saved only after completing the initial update or configuration.

** (see Upgrade Firmware)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.