DOCA0098EN-11

Summary Device View

Summary Device View provides summaries of one or more selected devices.

The measurements displayed in each summary are listed below.

Summary Measurement
Circuit
  • Demand RMS Current (A)
  • Active Power (kW)
  • Power Factor
  • Breaker Status
Load Current RMS Current per phase (A)
Demand Current RMS Demand Current per phase (A)
Power
  • Present Demand (kW)
  • Peak Demand (kW)
  • Recorded Time and Date
Energy Delivered
  • Active Energy Delivered (kWh)
  • Reactive Energy Delivered (kVARh)
  • Active Energy Total (kWh)
  • Reactive Energy Total (kVARh)
Energy Received
  • Active Energy Received (kWh)
  • Reactive Energy Received (kVARh)
  • Active Energy Total (kWh)
  • Reactive Energy Total (kVARh)
Power Quality
  • Power Factor Total
  • Frequency (Hz)
  • THDVLL (V)
  • THDVLN (V)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.