DOCA0098EN-11

Single Device View

Single Device View displays the following information for the selected device.
Menu Description
Monitored Area Parameters describing the location and use of the device as defined in Common Properties
Gauges

Analog view of device readings.

Options are Load Current (A), Power, Voltage LL, and Voltage LN.

Basic Most common readings for the selected device.
Energy Table view of energy data.
Demand Table view of power demand data.
Power Quality Table view of power quality data.
** Common Properties
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.