DOCA0098EN-11

Custom Page Management

You can create and add custom web pages to the Com’X to provide building overviews.

This section discusses how to add custom pages to the Com’X. For information on APIs and how to create a custom page, see the Com'X 510 Custom Web Page Technote, 7EN72-0199.

WARNING
INACCURATE DATA RESULTS
  • Do not incorrectly configure the software, as this can lead to inaccurate reports and/or data results.
  • Do not base your maintenance or service actions solely on messages and information displayed by the software.
  • Do not rely solely on data displayed in the software to determine if the device is functioning correctly or meeting all applicable standards and requirements.
  • Do not use data displayed in the software as a substitute for proper workplace practices or equipment maintenance.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.