DOCA0098EN-11

Define the Transfer Protocol

There are different protocols that you can use to export data.

The protocols in the Protocol drop-down list vary depending on the selected platform, as shown in this table:

Platforms Supported Transfer Protocols File Format
Energy Operation
  • FTP
  • HTTP and HTTPS
XML
Digital Service Platform Automatically defined by the Com’X EWS
CSV export
  • FTP
  • HTTP and HTTPS
  • SMTP
CSV

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.