DOCA0098EN-11

Predefined Events

Predefined Events are defined in the Com’X for protection devices. Enabling Predefined Events allows Facility Expert users to send event information from Com’X to Facility Expert.

Your Schneider Electric Partner can help you understand how to use these events to signal pre-trip conditions, analyze trips, and schedule periodic maintenance.

Predefined Events cannot be edited or acknowledged from the Com’X.

To enable/disable predefined events, click Settings > Events > Event Settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.