DOCA0098EN-11

Publication

Use the Publication subtab to select the platform to which the logged data is sent.

The Com’X can publish data to three different Schneider Electric platforms (database servers):

  • Energy Operation
  • Digital Service Platform (DSP)
  • CSV Export

The Com’X exports the data in the correct file format according to the selected platform. Then the data can be analyzed in the service to which you have subscribed.

The subscription to Energy Operation or DSP must be set up with a Schneider Electric representative before setting up the Com’X Destination platform.

To publish to DSP, you must enable Schneider Electric Services in Settings > General Settings > Schneider Electric Services.

With CSV Export, the Com’X exports data to your own database server in a .csv file.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.