DOCA0098EN-11

User Management

User Management allows you to create user groups with configurable permissions for Com’X features.

Then you can create individual user accounts and assign each user to a group, based on the desired permissions.

Only an administrator can add, modify, or remove users and groups.

** See Group Settings to configure user groups. See Users to add users.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.