DOCA0098EN-11

Users

There are two default users: admin and guest. An administrator can create additional users and assign permissions.

The table below describes login credentials for users.

Username Password User Group
admin

Default: admin

After the first time logging in, the user is prompted to change the password.

administrator
guest

Default: guest

Only an administrator can change the guest password. Admin user can change the guest password during initial configuration.

guest
User-defined An administrator assigns an initial password. The user must change the password after logging in. User-defined

Below is the interface to add, modify, or delete a user.

  1. Users: List of users for the Com’X. The format for users is Login ID (First Name Last Name).

  2. Login Information:

    • Login ID is the unique identifier for the account.
    • Group determines the permissions you want the user to have.
    • An administrator assigns an initial password.
  3. User Information: Includes user's first and last name and email address (optional).

** Related link: (see Group Settings).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.