DOCA0098EN-11

Checklist Before Leaving Customer Site

Schneider Electric recommends using this checklist before leaving customer site.

This list is not exhaustive.

Checkpoint Done Comments
Logging is ON in the banner.    
Publication is ON in the banner (if applicable).    
Each meter returns relevant values in the Measurements Table and Real Time Data tabs.    
Each analog sensor returns relevant values in the Measurements Table.    
No notification icon is in the Measurements Table.    
For Ethernet connections, the LED eth1 and/or eth2 is blinking.    
For GPRS or 3G connections, the wireless connection has a reception level at least equal to 2/4.    
For GPRS or 3G connections, check the LED and the general status.    
For Wi-Fi connections, the wireless connection has a good reception level.    
For Wi-Fi connections, check the LED and the general status.    
The last publication to the platform has to be successful (if applicable).    

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?