DOCA0098EN-11

Reboot Cases

Changing some Com’X settings can cause an automatic reboot.
Initial Network Configuration New Network Configuration
2 separate ports
  • 2 switched ports
  • GPRS/3G and 2 switched ports
  • Wi-Fi and 2 switched ports
GPRS/3G only
  • 2 switched ports
  • GPRS/3G and 2 switched ports
  • Wi-Fi and 2 switched ports
Wi-Fi only
  • 2 switched ports
  • GPRS/3G and 2 switched ports
  • Wi-Fi and 2 switched ports
2 switched ports
  • 2 separate ports
  • GPRS/3G only
  • Wi-Fi only
GPRS/3G and 2 switched ports
  • 2 separate ports
  • GPRS/3G only
  • Wi-Fi only
Wi-Fi and 2 switched ports
  • 2 separate ports
  • GPRS/3G only
  • Wi-Fi only
NOTE: It is recommended to use an external cellular router instead of the GPRS/3G configurations. Please refer to GPRS/3G Settings to see a list of recommended external 3G modems.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.