DOCA0098EN-11

Discovered Modbus Device Status

Discovered devices can have different status.
Message Description
OK The device is discovered and supported by the Com’X..
This device is already connected The device has been discovered from a previous Modbus discovery or by manual entry. It is supported by the Com’X.
Unknown device The device has been discovered but it is not supported by the Com’X. This occurs if the device is a custom device, and no custom models have been created in the Custom Library.
No device discovered No device is connected to this Modbus address (slave ID).
Refer to Modifying a Device to change the device settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.