DOCA0098EN-11

Ethernet Device Configuration Parameters

There are a set of parameters for an Ethernet device connected to the Com’X.

This table shows how to configure Ethernet devices:

Field Description
Host Defines the IP address of the device.
Port

Defines the port number.

502 is used for Modbus.

Slave ID

Gives the address only for Modbus TCP meters or devices.

Local ID

The address to use when accessing data from a device by an external client. The Local ID must be unique.

This configuration parameter can only be changed if data logging is disabled for the device being updated.

See Starting the Data Logging.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.