DOCA0098EN-11

Network Statistics

Your device provides network statistics.
Parameter Description
Ethernet
Speed

A status string that represents the speed setting being used to communicate with the linking partner.

Options: 10 Mbps or 100 Mbps

Duplex

A status string that represents the duplex setting.

Options: Full-Duplex or Half-Duplex

Collisions A counter that increments each time a frame is retransmitted due to collision detection.
CRC Errors A counter that increments each time a frame is received that has a checksum/CRC that does not match what is calculated.
Frame Errors A counter that increments each time a receive frame error is detected.
Packets Received OK A counter that increments each time a packet is successfully received.
Receive Packets Dropped A counter that increments each time a receive packet is dropped.
Receive Errors A counter that increments each time a packet is received with a receive error.
Packets Transmitted OK A counter that increments each time a packet is successfully transmitted.
Transmit Packets Dropped A counter that increments each time a transmit packet is dropped.
Transmit Errors A counter that increments each time a transmit packet experiences a transmission error.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.