DOCA0098EN-11

User Interface Features

The user interface organizes the features in main tabs and subtabs.
Main Tab Subtab Description
Settings General Settings Configures the date and time, network settings, proxy settings, publication parameters, and Wi-Fi access point settings.
Site Settings
  • Contains the name of the site. This field is used by Energy Operation.
  • Configures the logging interval for each commodity and for environmental parameters.
Communication Configures the Modbus serial port, Modbus gateway, TCP/IP filtering, and advanced Ethernet settings. Setup and create a ZigBee network.
Security Update SSL certificate and firewall settings.
User Management Create and edit groups and users.
Links Configure file and URL documentation links.
Events Configure event settings and define custom events.
Custom Page Management Create and add custom web pages to the Com’X.
Device Settings Configures the metering architecture and the data to log and publish.
Measurements Table Displays meters with metadata and data to be logged.
Commissioning
  • Checks the system configuration.
  • Starts or stops data logging.
  • Starts, stops, or tests data publication.
Monitoring Real Time Data Provides basic readings of selected devices. Features include single device and summary views.
Dashboards Provides graphical representation of energy consumption information aggregated over time for devices enabled for data logging and provides trending information for other electrical properties.
Control Device Resets Allows execution of resets defined for the device, and displays the date and time each reset function was performed.
Set Device Time Date and time resets are shown only when the device supports them.
Diagnostics Statistics Displays diagnostic data used to troubleshoot network problems.
Read Device Registers Allows users to read register data from local and remote Modbus devices connected to the Com’X.
Communications Check Tests the communications health of Modbus devices configured on the Com’X.
Custom Library
  • Create a custom device model, new device model or based on an existing custom device model in the library.
  • Modify and delete custom models
  • Import and export custom models.
Maintenance Logs

Shows the date, time, and description of:

  • changes in the configuration
  • errors detected during logging
  • publication steps and status
  • communication interruption with metering devices
  • unsuccessful login attempts
System Settings
  • Allows you to back up and restore a Com’X configuration.
  • Activates the remote access for Schneider Electric technical support.
  • Upgrades the Com’X firmware.
  • Allows you to manually restart the Com’X.
Events
  • Provides log of all generated pre-defined events.
  • Provides log of all pre-defined events to be published.
cross reference to settings, device settings, measurement table, commissioning, monitoring, control, diagnostics, custom library and maintenance
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.