DOCA0098EN-11

User Interface Overview

The web user interface allows you to commission your Com’X 510

This graphic shows the interface layout:

  1. Banner

  2. Gateway status

  3. Generic information

  4. Main tabs

  5. Subtabs

  6. Action buttons

Banner

The banner displays the following information at the top of all pages:

Status Data Logging: Displays status of data logging, which can be activated in the Commissioning tab.
Periodic Publication: Displays publication status, which can be activated in the Commissioning tab.
Available Storage: Shows available storage for data logging.
Generic Information Username/admin link: Displays the connected user.
About: Click to access information on your Com’X 510 and GPRS or 3G modem (serial number and MAC address), IPv4 Ethernet ports, IPv6 address, and software versions.
Logout: To log out of the session, click Logout or close your browser. It is recommended to log out of the Com’X 510 when not in use.
Time: Displays the time as set in the Date/Time Settings.

Main Tabs and Subtabs

Subtabs display the submenus under the selected main tab. You can use your web browser to bookmark each subtab of the Com’X 510 web interface.

Action Buttons

The action buttons correspond to the selected tab and vary. This table describes the interface buttons:

Button Action
Save changes

Validates the modifications. Disabled when:

  • there is no change in the web page.
  • a mandatory field is left blank. The field is highlighted in red.
  • inappropriate characters are entered in a field. The field is highlighted in red.

Cancel Cancels the modifications to return to the last saved settings.

Icons

Icon Description
Indicates that the information necessary to complete the energy server configuration and activation of data logging and publication is unavailable for the tab.
* Fields marked with a red star are required fields.
Indicates the user that is logged in for the current session.
Contains information about configuration in the open menu.
**See Features for a list of main tabs and subtabs. (see Configuring Date and Time Settings
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.