DOCA0098EN-11

HTTPS Connection

Your connection to the Com’X web server is HTTPS by default.

The Com’X has a self-signed security certificate. Therefore, connecting to the Com’X interface displays a security message. Before accepting, confirm that communication with the Com’X has been established.

HTTPS Redirection is enabled by default. It is recommended to leave this setting enabled to secure communications between PC and the Com’X.

HTTPS Proxy is supported in Settings > General Settings. The proxy address and port number are provided by your network administrator, or you can retrieve these values in the Internet Options of a PC connected to the LAN.

** To install a new certificate, see Uploading a New Certificate. See Configuring Proxy Settings
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.