DOCA0098EN-11

Secure Data Export

Using a secure protocol when publishing data logs can help prevent interception and corruption of data logs.

Secure publication options include: 

  • HTTPS when publishing data as a .csv file or publishing to Energy Operation.
  • SMTP with connection security mode to TLS/SSL or STARTTLS when publishing a .csv file over SMTP. The default mode is None.
  • DSP (a Schneider Electric hosted platform)

Destination platform is not configured by default. If you are publishing to a location other than DSP, you must configure the protocol in Settings > General Settings > Publication, then Email Settings if using SMTP.

** See Define the Transfer Protocol and Configuring the SMTP Server.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.