DOCA0098EN-11

User Management

User Management allows you to create user groups with configurable permissions for Com’X features. You can restrict access to features by assigning individual users to a group.

There are two default groups: 

  • administrator: Modification rights for all features; you cannot modify this group.

  • guest: Viewing rights for selected features. Only an administrator can modify this group.

Only an administrator can add, modify, or remove users and groups.

** See User Management
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.