DOCA0098EN-11

Port Settings

There are default Firewall Management settings for each protocol per interface.
  Ethernet 1 Ethernet 2 Wi-Fi GPRS/3G
HTTP 80, Enabled 80, Enabled 80, Enabled 80, Disabled
HTTPS 443, Enabled(1) 443, Enabled(1) 443, Enabled 443, Disabled
Modbus TCP 502, Disable 502, Enabled 502, Enabled 502, Disabled
(1) Cannot be updated.
NOTE: Refer to Security Configuration Recommendations for additional information regarding risks associated with unsecure protocols and recommended best practices.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.