DOCA0098EN-11

Publication Identification Settings

There are publication identification settings for Energy Operation.
Field/Button Description
Publication ID

This number is a unique identifier of the site for the Energy Operation database. It is used to create a site in Energy Operation.

This ID is automatically generated by the Com’X.

Generate new publication ID

This button generates a new publication ID number. Use this button whenever you reuse:

  • the Com’X for a new site.
  • the current Com’X configuration on a different site.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.