DOCA0098EN-11

Digital Service Platform Connection

**
To publish to DSP, you must enable Schneider Electric Services in Settings > General Settings > Schneider Electric Services.

Each state of connection to Digital Service Platform is confirmed with a green check mark when enabled or grayed out when disabled. A red check mark indicates an issue with the specific connection state. The three connection states are:

Initialize – DSP agent initialized.

Authenticate – DSP connection authenticated.

Connect – DSP connection complete, and device has been identified on the remote platform.

NOTE: Maintenance logs record Schneider Electric Services state changes.

When using the DSP connection, firmware upgrades are automatically launched. It is recommended that you update the firmware if you want to use the DSP platform through a slower GPRS connection.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.