DOCA0098EN-11

Network Troubleshooting

There are some tips for troubleshooting your network.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • This equipment must only be installed and serviced by qualified personnel.
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E in the USA, CSA Z462 or applicable local standards.
Failure to follow these instructions will result in death or serious injury.

Ethernet Troubleshooting

This table describes how to solve issues with Ethernet.

Issue Possible Solution
Ethernet LEDs are not blinking. Check that the Ethernet LAN cables are not disconnected.
Cannot access to Modbus devices downstream from a Modbus TCP/Modbus serial line gateway. Check the IP address of the gateway. If data export is via GPRS/3G, check that the gateway is on the same Ethernet subnetwork as the Com’X.

GPRS/3G Troubleshooting

This table describes how to solve issues with GPRS or 3G.

Issue Possible Solution
Modem is not detected. The LED modem is not flashing. Power down the Com’X. Reinsert the modem and power up the Com’X.
Modem cannot connect to the network. Check that the settings such as the APN are correct.
GPRS LED on front panel turns ON and OFF periodically. Check that protocol settings are correct in General Setting > Publication.

Wi-Fi Troubleshooting

This table describes how to solve issues with Wi-Fi.

Issue Possible Solution
Wi-Fi USB key is not detected. The USB key LED is not flashing. Power down the Com’X. Reinsert again the Wi-Fi USB key and power up the Com’X.
Wi-Fi USB key cannot connect to the network. Check that the settings such as the SSID name and the WPA2 key are correct.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.