DOCA0098EN-11

Com’X Troubleshooting

**3 xrefs in this topic
com’x access: follow procedure Logging In for the First Time, follow procedure for Resets.

Com’X Access

Issue Possible Solution
Cannot log in through customer LAN. Log in to the Com’X. Check the IP address.
Lost password Follow the procedure to reset the password.

Web Pages

Issue Possible Solution
The web pages are not displayed correctly. Check the screen resolution of your laptop. It must be set to at least 1280x1024.
In Internet Explorer, check that the Display intranet sites in compatibility view box is disabled by selecting View settings compatibility in the Tools tab of Internet Explorer.
Delete browsing history.

Digital Service Platform Selection

Issue Questions to be asked Possible Solution
Authentication Issue

Was the Com’X connected to DSP prior to the issue?

Is this a duplicated Com‘X or has the Com’X been factory reset?

If yes, then restore configuration on the Com’X.

If yes, then contact Schneider Electric Services.

Unable to connect to Digital Service Platform after configuring proxy.

N/A

Disable and enable Schneider Electric Services.

Unable to set date/time on the Com’X.

Is Com’X connected to Digital Service Platform ?

If yes, then wait for the date and time to get synchronized and display.

unsuccessful publication with Eth/wifi: see Proxy Settings.

Data Publishing

Issue Possible Solution
Publication to the platform was unsuccessful.

  • Check the platform user name and the password.
  • Check the Com’X date and time.

Publication to the platform was unsuccessful with Ethernet or Wi-Fi. Check if a proxy is implemented on the network.
The Com’X connects to the FTP server but does not succeed in delivering the data file. Check that your FTP account has the right to rename a file on the FTP server.

Firmware Upgrade

Issue Possible Solution
Firmware is not upgraded when managed through USB memory key plugged on front panel. Delete the file DNxxxxxxxxxxxxx-xxx (where xxxxxxxxxxxxx-xxx is the serial number of the Com’X) registered at the root directory of the USB memory key.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.