DOCA0098EN-11

Recreating a ZigBee Network

Use this procedure to change the channels on a ZigBee network that has already been created for the Com’X.

When you perform this procedure, all equipment that is connected to the ZigBee network is disconnected. You must use the ZigBee discovery function to reconnect devices to the network.

  1. Log in to the Com’X, and then select Settings > Communication > ZigBee Settings.

    The ZigBee Settings screen is displayed.

  2. In the Activate ZigBee field select No, and then click Save changes.

    The ZigBee status shows that no network is defined. You can now perform maintenance or change the network settings.

  3. In the Activate ZigBee field, select Yes.
  4. In the Create New ZigBee network field, select Yes.
  5. Follow step 6 through to the end of ZigBee Network Settings to complete the setup.
**ZigBee Network Settings (**ZigBee Device Discovery)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.