DOCA0098EN-11

Retrieving Proxy Values

You can retrieve your network proxy values in Internet Explorer.

This graphic shows the interface to retrieve proxy values from Internet Explorer:

  1. Connections tab

  2. Local Area Network (LAN) settings

  3. Proxy server with address and port

  1. Click the Tools menu.
  2. Select Internet Options in the drop-down list.
  3. Select the Connections tab.
  4. Click the LAN settings button.
  5. Read the values of the proxy in the Local Area Network (LAN) Settings window.
  6. Copy the same values into the Com’X proxy settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.