DOCA0098EN-11

Starting the Data Logging

You need to start data logging on your energy server for it to log data.
Before you can log data, you must:
  • complete configuration of the Com’X.
  • configure the devices that you want to log data .
  • select the data to be logged.
  1. Click Commissioning > Data Logging.
  2. Click Start data logging.

    The date and time that logging is initiated are displayed.

To disable data logging, click Commissioning > Data Logging > Stop data logging.

**(see Manage Devices) (see Selecting Measurements to Publish)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.