DOCA0098EN-11

Configuring Access Settings with EBXA-GPRS-SIM Card

You can only use the EBXA GPRS SIM to publish data if you are exporting data to Digital Service Platform.
This is a poorly formed task and should be rewritten when project/time allows.

The SIM card is embedded in the GPRS modem. The access settings of this GPRS modem are set by the Com’X.

The reference EBXA-GPRS-SIM must be selected for this GPRS modem.

NOTE: It is recommended to use an external cellular router instead of the EBXA-GPRS-SIM. Please refer to GPRS/3G Settings to see a list of recommended external 3G modems.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.