DOCA0098EN-11

Configuring Access Settings with EBXA-GPRS or a 3G Modem

You need to configure access settings when using an EBXA-GPRS or 3G modem.

Install the SIM card into the GPRS modem as described in the EBXA-GPRS/EBXA-GPRS-SIM Instruction Sheet, reference 253537613. For 3G, install the SIM card into the 3G modem as described in the manufacturer's installation instructions.

The EBXA-GPR/3G modem requires:

  • a mini SIM 2FF type card.
  • a minimum 1 MB/month data export on the telecom contract.

A robust M2M SIM card is recommended rather than a standard SIM card.

NOTE: It is recommended to use an external cellular router instead of the EBXA-GPRS. Please refer to GPRS/3G Settings to see a list of recommended external 3G modems.
  1. Click Settings > General Settings > Network Settings.
  2. Select EBXA-GPRS/3G.
  3. Type the APN, Username, Password, and PIN Code provided by the access provider.
  4. Click Save changes.
NOTE: The PIN code and the password of the SIM card cannot be changed by the energy server.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.