DOCA0098EN-11

Configuring the Ethernet Ports

You can configure the Ethernet ports to as two separate ports.
  1. Click Settings > General Settings > Network Settings.
  2. Select the Choose your network configuration field.
    NOTE: If you change the configuration of the Ethernet port you are configuring through, you will be disconnected through the browser. Begin a new browsing session to continue configuration.
  3. Select 2 Separate Ports (1 IP address for each) in the drop-down list.
  4. Select DHCP client and Static IPv4 address in the Configuration mode drop-down list.
  5. In the Ethernet configuration collapsible menu, enter the parameters in the WAN network configuration (eth1) and LAN network configuration (eth2) fields.

    The Interface Status field changes to ACTIVE (if correctly wired).

  6. In General network settings collapsible menu, type the addresses in the Default gateway, Primary DNS server, and, if necessary, Secondary DNS server fields.

    Addresses are assigned to the Com’X by the IT administrator.

  7. To enable ping replies, select Yes in General network settings > Reply to ping.

    Reply to ping is disabled by default.

  8. Click Save changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.