DOCA0098EN-11

Configuring Modbus Serial Port Settings

You can configure Modbus serial port settings on your Com’X.
NOTICE
Impaired Network Performance
Only qualified workers should modify the Modbus gateway settings. Such modifications should be performed only after reading about and understanding the Modbus gateway settings.
Failure to follow these instructions can impair network performance.
  1. Click Settings > Communication > Modbus Serial.
  2. Select the required value in the Baud rate drop-down list.
  3. Select the required value in the Parity drop-down list.
  4. Select the required value in the Number of stop bits drop-down list.
  5. Select the required value in the Timeout drop-down list.
  6. Select Yes in the Terminator resistance field if the bus is terminated at its end
  7. Select Yes in the Serial line polarization field if no other device in the line is providing polarization.
  8. Click Save changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.