DOCA0098EN-11

Configuring Proxy Settings

**need 210 topic, or delete graphic
You can configure the Internet proxy settings, if required.
The proxy address and port number are provided by your network administrator, or you can retrieve these values in the Internet Options of a PC connected to the LAN.
  1. ClickSettings > General Settings > Proxy Settings.
  2. Select the HTTP Proxy settings or HTTPS Proxy settings field.
  3. Select the Enable HTTP proxy support check box.
  4. Type the address and port of the proxy in the Proxy address and Proxy port fields.
  5. If proxy authentication is required, select Yes for Proxy requires authentication, and enter the login and password to the proxy.
  6. Click Save changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.