DOCA0098EN-11

Creating a Custom Model

To use a custom model, you must first create a new custom model.
  1. Click the Custom Library main tab.
  2. Click +Create on the lower left part of the page.

    The Create a custom model dialog opens.

  3. Enter the following settings:
    Field Setting
    Select model type Select a model type from the list. This selection determines the properties structure of the new custom model.
    Create model

    Select the basis for the new custom model:

    • New
    • Based on a Schneider Electric model
    • Based on a custom model

    <base model type> If you are basing the new custom model on an existing Schneider Electric model or a custom model, select the existing model on which the new model is based.
    Model name Enter the name of the new custom model, or accept the default name.
    Default value of commodity Select a default commodity the new model measures.
    Default value of usage Select a default value for how the new model is used
  4. Click Create.

    The dialog closes, and the newly created custom model properties page opens for initial configuration.

Either add related topics or rework this sentence.Refer to the following topics for a description of custom model properties configurations.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.